Technical FAQs

Ask a Question

What are the differences between T200I and T200E

Functionally there are no differences between the two RTU's.

The key differences are: -

  • IP rating of T200I is IP41
  • IP rating of T200E is IP54
  • T200E is limited to controlling 4 functions
  • T200E can control up to 16 functions
  • T200I has Harting type connectors underneath the cubicle for the switchgear umbilical's
  • T200E has special sockets inside the cubicle on the interface card


For more information on T200I click here and T200E click here

Was this helpful?
What can we do to improve the information ?