Technical FAQs

Ask a Question

What is the IP rating of the XVC complete (monolithic) tower beacons?

The degree of protection conforming to EN/IEC 60529 is;

When mounted on support tube;
  • IP54 (Flat surface installation)
  • IP23 (Vertical surface installation)
When mounted on base;
  • IP54 (Flat surface installation)

Note: If a tower beacon with a higher IP rating is required, consider using the XVP diameter 50mm range that has an IP65 rating (for illuminated units, IP43 for audible units).
Was this helpful?
What can we do to improve the information ?