Technical FAQs

Ask a Question

What is the temperature class of insulation for a liquid immersed Power Distribution Transformer ?

The temperature class of insulation for a Liquid Immersed Power Distribution Transformer is Class A  in accordance with IEC 60085 "Recommendations for the Classification of Materials for the Insulation of Electrical Machinery and Apparatus in Relation to their Thermal Stability in Service
Was this helpful?
What can we do to improve the information ?