Technical FAQs

Ask a Question

What is the temperature class of insulation for a Trihal Cast Resin Transformer

The temperature class of insulation for a Trihal Cast Resin Transformer is Class F  in accordance with IEC 60085 "Recommendations for the Classification of Materials for the Insulation of Electrical Machinery and Apparatus in Relation to their Thermal Stability in Service"
Was this helpful?
What can we do to improve the information ?