Technical FAQs

Ask a Question

How many Low Voltage cables can be connected to the phase and neutral terminals of a Fast Trans Transformer ?

The Fast Trans range of transformers which are liquid filled free breathing distribution transformers covers 8 kVA ratings and the number of Low Voltage cables that can be connected within the LV cable box varies for each rating as detailed below :-

315kVA     One single core cable per phase and one on the neutral ( 4 single core cables total)

500kVA     One single core cable per phase and one on the neutral ( 4 single core cables total)

800kVA     Two single core cables per phase and one on the neutral ( 7 single core cables total)

1000kVA   Two single core cables per phase and one on the neutral ( 7 single core cables total)

1250kVA    Two single core cables per phase and one on the neutral ( 7 single core cables total)

1500kVA    Three single core cables per phase and two on the neutral ( 11 single core cables total)

1600kVA    Three single core cables per phase and two on the neutral ( 11 single core cables total)

2000kVA    Four single core cables per phase and two on the neutral ( 14 single core cables total)

The above number of LV cables are the standard arrangement - should alternative cable arrangements be required then this should be discussed at the time of tender

Was this helpful?
What can we do to improve the information ?