Technical FAQs

Ask a Question

By how much is the operating current of an LC1 BP contactor increased if two poles are connected in parallel?

The switching capacity is increased by 1.6 times the nominal current (at AC1 duty only), see the attached file.
Was this helpful?
What can we do to improve the information ?