Technical FAQs

Ask a Question

What Safety Relay should I use with a Two Hand Control Station?

Safety modules XPS BA, BC and BF may be used for two-hand control stations in order to comply with the requirements of European standard EN 574/ISO 13851 for two-hand control systems.

Below is a table showing which of the Safety Relays is required to achieve the Requirements for the Safety Standards EN954-1

Was this helpful?
What can we do to improve the information ?