Technical FAQs

Ask a Question

What is the maximum operating rate of an LC1 BL contactor?

The maximum operating rate of an LC1BL contactor is 120 cycles per hour (@ less than 55 degC).
Was this helpful?
What can we do to improve the information ?