Technical FAQs

Ask a Question

What standards cover Mineral Oil used in Power Transformers

The International Standard for "Unused Mineral Insulating Oils for Transformers and Switchgear"  is  IEC60296:2003

The British Standard for "Unused Mineral Insulating Oils for Transformers and Switchgear"  is  BS EN 60296:2004

Reclaimed mineral oil is covered by BS 148:2009 "Reclaimed mineral insulating oil for transformers and switchgear"
Was this helpful?
What can we do to improve the information ?