Technical FAQs

Ask a Question

What are the main reference standards (International and National) applicable to Power Transformers ?

The main International Standard for Power Transformers is IEC 60076

The British Standard for Power Transformers is BS EN 60076
Was this helpful?
What can we do to improve the information ?