Technical FAQs

Ask a Question

What is the differences within the TSXETG3000 Ethernet Gateways product range?

These products are free standing modules that can be implemented into an Ethernet Network. All of these modules require configuration with Web Designer software supplied with module. The units are classed as Factory CAST HMI products as they can have custom web pages added, . Custom web pages can be created using Microsoft Front page. The TSXETG3000 range of gateway are all Class D20 embedded web server. Factorycast HMI adds servcies such as E-mail,

They included a gateway to enable you to connect onto either a Unitelway bus, or Modbus bus depending upon the hardware you use :-

TSXETG3000 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality, configured with Web Designer s/w supplied with module

TSXETG3010 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality + PSTN Modem and embedded I/O board

TSXETG3021 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality+ GSM Modem 900 / 1800MHz (UK and European Market) and embedded I/O board

TSXETG3022 Ethernet (Modbus TCP/IP Network) to Modbus RTU gateway functionality + GSM Modem 850 / 1900MHz (US and Canada and South American Market) and embedded I/O board.

For further details see summary of funcitons document attached.

Was this helpful?
What can we do to improve the information ?