Technical FAQs

Ask a Question

What contact configurations are available on ABR Electro mechanical interface relays?

Various contact configurations are available to suit the customer application  :-

1 N/O (Normally Open)
2 N/O
1 C/O (Change over with common)
1 N/O + 1 N/C (Normally Open + Independent Normally Closed)
Was this helpful?
What can we do to improve the information ?