Technical FAQs

Ask a Question

What are the supply voltage options for Magelis iDisplay?

The supply voltage must be between 100 to 240Vac (98 - 264Vac including tolerance) compliant with EN 61131-2
Was this helpful?
What can we do to improve the information ?