Technical FAQs

Ask a Question

How many I/O signal channels does the ABE9 product range support?

There are two sizes 4 channel or 8 channel. Each channel is connected via a 5 pin M12 female connector on base (IP67).
Was this helpful?
What can we do to improve the information ?