Technical FAQs

Ask a Question

I need to control the level of a liquid in a tank, what can I use?

We have several options from the Zelio Control range

For Rail Mounted solution
The RM4L Liquid level control relay in combination with a Level control probe LA9RM201 or a series of probes.
This unit can have a built-in time delay function, dependent upon the unit selected

For Plug in type solution
The RM84870*** Liquid level control relay in combination with a RUZ1A base and a series of probes.
This unit can also perform Empty / Fill functions
Was this helpful?
What can we do to improve the information ?