Technical FAQs

Ask a Question

Why I cannot communicate with a Power Meter (PM710 or PM750) from a remote personal computer?

Possible Cause

The Power Meter address is incorrect

Possible Solution
Check that the Power Meter is correctly addressed, each meter on the same bus should have a unique address.

Possible Cause

Power Meter baud rate is incorrect

Possible Solution
Verify that the baud rate of the power meter matches the baud rate of all other devices on its communication link.

Possible Cause

The parity is incorrect

Possible Solution
Check the parity on all the meters are the same on the communication link.


Was this helpful?
What can we do to improve the information ?