Technical FAQs

Ask a Question

What is the default password for the PM700 Power Meter range ?

To begin power meter setup, do the following:

1. Press ...>  until you see SETUP
2. Press SETUP
3. Enter your password.

The default password is 00000.

If this password has been changed please make sure you make a note of the new password as it cannot be reset

Was this helpful?
What can we do to improve the information ?