Technical FAQs

Ask a Question

Why can't I find combination Motor Starters (eg GV2DM202) on the My Schneider site?

In the UK we do not offer pre-assembled  combination starters, but the individual parts to make them up (assembly requires literally seconds).

Each starter is made up of  a GV2 manual motor starter and a contactor (LC1D or LC1K) plus an adaptor to join the two together. The section of the catalogue dealing with combination starters lists the numbers of the individual parts required.

D.O.L Revering starter GV2DM202**

This is made from
Motor Circuit Breaker GV2ME02
Contactor LC2D09**
Combination Block GV2AF3

** refers to the coil voltage code eg BD for 24Vdc
Was this helpful?
What can we do to improve the information ?