Technical FAQs

Ask a Question

How far apart should you place the fixing brackets when installing KBA, KBB, KNA & KSA busbar

In general we would normally recommend 3m centres between brackets when installed on edge using the universal fixing brackets.
The KNA range when installed on flat should be 1.5m maximum and 2m maximum for the KSA range.
Was this helpful?
What can we do to improve the information ?