Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Electrical distribution | Intelligent lighting control | C-Bus intelligent lighting control

C-Bus intelligent lighting control

C-Bus gives you full control of your building environment at the simple touch of a button or via a web page, accessible from any networked terminal in the building. Based on a simple, extendable, and easy to install solution, C-Bus gives you a platform that ensures you get the best out of your building environment.

Units on the C-Bus Network have their own built-in microprocessor, allowing them to operate independently with "distributed intelligence”. This means that the unlikely malfunction in one unit will not affect the operation of any other Unit or the Network. A network consists of building blocks allowing fast and reliable operation to each C-Bus device.

 
Input units include:
Key Input Touch Screen
  • Key input, touch screen
  • Analogue/digital input
  • Passive infrared, light level, temperature sensors
 
Output units include:
Dimmer Output unit
  • Dimmer
  • Relay
 
System units include:
Network Interface Unit
  • PC interfaces
  • Ethernet network interfaces
  • DALI gateways
 

Using an unshielded twisted pair ‘Cat 5’ cable, the C-Bus Network not only provides the means of communication between units, but also the small amount of power needed to operate the circuitry within each C-Bus unit. More information…

Visit the Inteligent lighting control application pages

 More information/downloads
View and download the C-Bus brochures
For more info download the 2007 Customer Training Brochure (0.8 Mb)