Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Products & Services | Electrical distribution | Consumer units

Consumer units

Domae & Qwikline II
 
Through the Square D brand Schneider Electric is a market leader in the design and manufacture of British Standard consumer units.

With the introduction of the 17th Edition Wiring Regulations, Domae and Qwikline II consumer units from Square D, a brand of Schneider Electric, have been specifically designed to accept additional new RCDs, MCBs and RCBOs to help ensure compliance to the 17th Edition of the wiring regulations. Being both quick and easy to install with all the safety features expected, Domae and Qwikline II offer onsite flexibility at very competitive prices. Each offers significantly different designs suitable for domestic dwellings and commercial and public buildings such as schools and hospitals.

The Domae consumer units are available with insulated or metal enclosures and can configured in several different ways to help compliance. In addition a new range of 1 module RCBO's are now available.

Supported by a network of nationwide stockists we provide two dramatically different styles of consumer unit, Domae and Qwikline II. Suitable for installation in domestic dwellings, schools, colleges, hospitals etc., - both offers provide high levels of quality and installer flexibility.
Domae consumer units
The Domae range of consumer units
Domae consumer units
offers the ultimate interms of onsite flexibility at a very affordable price. Available with insulated or metal enclosures there are no bespoke split load consumer units. However, any Domae enclosure can be taken and used with a single incomer or converted to a split load board with the minimum of effort ...
 
Qwikline II consumer units
The Qwikline II range of consumer units provides
Qwikline II consumer units
arguably the highest levels of residential circuit protection safety. A wide range of switch disconnectors, RCDs and MCBs is also complimented by an SP RCBO offer for maximum continuity of supply in the event of a fault. What sets Qwikline apart is the plug-on breaker concept and fully encapsulated busbars...
     
     
     
     
 More information/downloads
For more info download the Domae and Qwickline II Consumer Units guide (0.6Mb)