Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Electrical distribution | Low voltage circuit breakers | A class SiE RCDs – LV Circuit Breakers – Electrical Distribution

 

 

A class SiE type Residual current devices


Residual current circuit-breakers for specific applications which ensure:

  • The control and isolation of electrical circuits
  • The protection of persons against direct and indirect contacts
  • The protection of installations against insulation faults.
A class SiE type RCDs

They conform to both the residual current device standard BS EN 61008 and to switch standards BS EN 60947-1 and BS EN 60947-3.

These Residual current circuit-breakers are used in the commercial and industrial sectors where many power supplies may be present and there is a risk of tripping due to:

  • Successive lightning strokes
  • IT earthing system
  • Variable speed controllers, frequency converters
  • Presence of electronic ballasts
  • Presence of switchgear that incorporates interference filters i.e. lighting, microcomputing, etc.

Plus the SiE type is humid environments and/or environments polluted by aggressive agents, for example swimming pools, marinas, the food-processing industry, water treatment plants, and many heavy industrial sites.

Technical data
  • Voltage rating 230…400 V AC, -15…+10 %
  • Frequency rating: 50/60 Hz
  • Current rating (Ith) at 40 °C 16…80 A
  • As in BSEN 61008 Breaking and making capacity Rated residual (I∆m): 2.5 kA Rated (Im): 1.5 kA
  • As in BSEN 60947-3: Isolation with positive break indication, opening is indicated by a green strip on the device operating handle. This indicator shows that all poles are open.
  • Rated impulse withstand Voltage (Uimp): 6 kV
  • Insulation voltage (Ui): 440 V
  • Utilisation category: AC 23A rating up to 63 A, AC 22B ratings 80
  • Padlocking in the "tripped" position is possible using the padlocking device (not supplied)
  • Protected against nuisance tripping due to transient overvoltages (lightning, switchgear operation on the network, etc.) Impulse withstand level 8/20 µs: 3 kA for instantaneous, 3 kA for selective.
  • Short-circuit current withstand (I∆c = Inc): 10 kA with 100 A fuse upstream
  • Number of operations (O-C): 20 000
  • Units with fixed sensitivities for all ratings
  • Instantaneous trip or Selective trip =  total vertical selectivity can be achieved using 30 mA residual current devices placed downstream
  • Mechanical Indication: earth fault indication on front panel by means of a mechanical indicator
  • Electrical Indication: using auxiliaries
  • Remote tripping: using auxiliaries ( shunt or undervoltage release)
  • Environment: Tropicalisation: treatment 2 (relative humidity 95 % at 55°C)
   
 More information/downloads
For more info download the RTI catalogue section 4 about protection (1.5Mb)
”Sales
 Sales support
”Product
 Product support ”Schneider   eLibrary literature