Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Automation Control | Safety components | Safety Dialogue

 

Safety Dialogue from Preventa Safety Solutions


Many safety process require interaction with the operator – whether starting or stopping a process, or providing feedback on machine status, Preventa gives you the widest range of choices to provide you with the best solution.
Safety dialogue devices can be split into three main categories:

Preventa Safety Solutions
Starting devices - footswitches, two hand control stations and enabling switches provide the operator with a number of methods to signal to the safety circuit that a process cycle may commence.
Two hand control stations and dedicated monitoring modules make sure that operators are clear of a process such as a press before the cycle commences, and are often required on certain applications to meet Type C safety standards. Enabling switches give operators local

control when entering dangerous areas, operating as a “dead mans handle” with hold to run operation and an additional stop function if the handle is squeezed. This is ideal in set up operations such as printing presses or robot cells.

Stopping Devices - devices to provide emergency stop signals include mushroom head pushbuttons and control stations from the Harmony range, and rope pull switches that can provide a similar function along the whole length of a conveyor or a machine whilst reducing the electrical circuitry and installation time required.

Indication Devices - beacons and sounders, also from the Harmony range provide simple and effective status of a machine to the operator from great distances. Available as either single, free standing devices or as modular, stackable systems such as the world leading XVB range, the range is adaptable to meet your application.

   
 More information/downloads
For more info download Preventa - The Essential Guide (3.6Mb)
 Sales support
 Product support  eLibrary literature