|
Unity
|
The future of automation lies in Unity
Schneider Electric has drawn on its expertise to develop Unity, a comprehensive family of Modicon Automation Controllers supported by a common suite of software tools.
With Unity and Transparent Ready, Schneider Electric truly takes you into a new world of automation: Collaborative Automation.
|
|
|
| |
|
Unity Software
Unity Pro IEC61131-3 Programming Software
|
|
|
Unity Pro is the all-in-one programming software common to the Modicon M340, Premium, Atrium and Quantum automation controllers. Fully compliant with IEC61131/3, Unity Pro keeps the best values of PL7 and Concept software and opens the door to a complete set of new features for greater productivity and openness.
Unity EFB Toolkit, Visual C++ developers can create tailor-made functions to be used within Unity Pro. |
|
|
Unity Specialised Software
|
|
 |
Unity Application Generator is the specialized software for design and code generation of batch/process type applications. UAG translates the customer specifications into automation control logic while providing a seamless PLC / HMI integration. By strictly applying the ISA S88 methodology, UAG drives development with more efficiency and provides a higher quality and viability of the installation. |
| |
 |
Unity Developer’s Edition includes additional software for IT development engineers in VBA, VB or C++. It provides local or remote access to all Unity Pro object servers. UDE is used within the Collaborative Automation Partner Program (CAPP) to develop connections with third-party software providers. It can also be used to develop customized and made-to-order solutions or automate repetitive tasks (data entry, configuration, translation, etc.). |
|
|
Unity Hardware
|
|
| Modicon automation controllers supported by Unity software offer you ingenuity, flexibility and openness for increased productivity of machines, industrial processes and infrastructures. The family consists of: |
|
| |
|
Modicon M340
Rugged, powerful and compact, the new Modicon M340 programmable controller is the ideal solution for machine manufacturers. Modicon M340 is also the ideal partner for Modicon Premium and Modicon Quantum to meet the automation requirements of industrial processes and infrastructures at the heart of Transparent Ready architectures.
|
|
|
 |
|
Modicon Premium
Compact, flexible and optimised for fast processes, Modicon Premium is the specialist automation controller for machines and manufacturing processes. By its capacity to integrate distributed architectures, Modicon Premium offers ideal solutions for infrastructures, particularly in water and transport. |
|
|
 |
|
Modicon Quantum
With a comprehensive catalogue of modules and an extended field bus and network communication offer, Modicon Quantum is perfectly adapted to the requirements of continuous and semi-continuous industrial processes, and to control of large infrastructure sites.
|
|
|
 |
|
Modicon Atrium
The Modicon Atrium offers the same performance and capabilities as the Modicon Premium processor, but all on a PCI bus card so that you can turn your PC into a PLC!
|
|
|
| |
|
| More information/downloads |
 |
|
For more info download the Unity Panorama Brochure (0.3Mb) |
 |
|
For more info download the Unity Pro Brochure (0.8Mb) |
 |
|
For more info download the Unity Application Generator Brochure (0.8Mb) |
 |
|
For more info download the 2007 Customer Training Brochure (0.8 Mb) |
 |
|
 |
 |
|
|
|