Modicon TSX Micro The Modicon TSX Micro offers tremendous flexibility in a compact design. Intended for smaller applications, this platform boasts integrated analogue and counter options to reduce costs, plus optional Ethernet connectivity. User-removable memory cards allow for easy maintenance and system expansion.
Type • Local I/O and Distributed I/O • Discrete, Analogue and Application specific Maximum Local I/O • Discrete: 248 • Analogue: 41 Maximum Distributed I/O • Discrete: Network dependant • Analogue: Network dependant