Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Automation Control | Distributed I/O & Interfaces | Advantys FTM

 

Advantys FTM

Modular block IP67 distributed I/O

       


Advantys FTM

Advantys FTM splitter boxes are designed for use in harsh environments providing direct connection of sensors and actuators at the heart of the process or machines. This modular offer enables, from a single fieldbus communication interface, the connection of a changeable number of discrete or analogue I/O splitter boxes, giving high I/O counts per node.


   
Key highlights:
  • M8 or M12 connector digital I/O modules (8 I, 16 I, 8 I/O, 16 I/O)
  • M12 connector, voltage or current, analogue I/O modules (4 I or 4 O)
  • Up to 256 discrete I/O per node
  • Support of IP67 analogue I/O splitter blocks
  • Diagnostic channel and integrated module
  • Compatibility with sensors and actuators with integrated diagnostics (DESINA)
  • Connectivity to fieldbus:
    CANopen, Profibus DP, DeviceNet
   
 More information/downloads
For more info download the Advantys range guide (3.5Mb)
”Sales
 Sales support
”Product
 Product support ”Schneider   eLibrary literature