Find
eCatalogue search
 
Direct links
DownloadsFind a DistributorFAQ'sMy Schneider Electric
 
Company
information
CareersAbout us
 
Around the world
Products & Services | Automation Control | Distributed I/O Input Output & Interfaces

Distributed I/O and Interfaces

The Advantys range of distributed I/O and interface products has been designed to meet the needs of all distributed architectures. Developed with environmental, architectural, cost and performance needs in mind, there is a solution available for virtually all kinds of application:
• Advantys Distributed Inputs/Outputs
• Advantys AS-Interface cabling system
• Advantys Telefast pre-wired system

Distributed architectures offer significant benefits over traditional centralised control: reduction of cabling, space, installation and commissioning costs along with simplification of maintenance and ease of system expansion.

Modular distributed I/O
Advantys STB is a distributed I/O platform
Modular Distributed I/O
providing a wiring solution, power management and device integration system all in one compact system...
 
Optimised distributed I/O
Open and modular, the Advantys OTB offer
Optimised Distributed I/O
is an ideal solution for “optimized” type distributed input/output requirements...
Simple block IP67
Distributed I/O

Compact and flexible,
Simple Block IP67 Distributed I/O
Advantys FTB splitter boxes are designed for use in harsh environments and can be mounted at the heart of the machine or process...
 
Modular block IP67
Distributed I/O

Advantys FTM splitter
Modular Block IP67 Distributed I/O
boxes are designed for use in harsh environments providing direct connection of sensors and actuators at the heart of the process or machines...
Advantys AS-Interface cabling system
The Advantys AS-Interface
Advantys AS-Interface Cabling System
modules (available as IP20 or IP67) enable standard automation products, such as push buttons or indicator banks to easily connect to AS-Interface...
 
Pre-wired interfaces
The Advantys Telefast pre-wired interfaces (IP20 and
Pre-Wired Interfaces
IP67) replace traditional panel terminal blocks by providing connection and adaptation of control signals to PLC I/O cards via pre-wired cabling arms...